imxrt1050 - Read uploaded prgram on flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imxrt1050 - Read uploaded prgram on flash

ソリューションへジャンプ
1,264件の閲覧回数
dynamix
Contributor II

hey folks,

I wanna make sure that some specific data are placed at some memory address on the flash. Is there any way for me to read the data stored on the flash?

Thanks,

ラベル(1)
0 件の賞賛
返信
1 解決策
1,255件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Dynamix,

A good starting point is looking at the examples available as part of the MCUXpresso SDK for the i.MXRT1050. There is an example that covers using a HyperFlasg with FlexSPI.

You can download the SDK from the MCUXpresso Builder:

https://mcuxpresso.nxp.com/en/select

I hope that this helps!

Regards,
Gustavo

元の投稿で解決策を見る

2 返答(返信)
1,256件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Dynamix,

A good starting point is looking at the examples available as part of the MCUXpresso SDK for the i.MXRT1050. There is an example that covers using a HyperFlasg with FlexSPI.

You can download the SDK from the MCUXpresso Builder:

https://mcuxpresso.nxp.com/en/select

I hope that this helps!

Regards,
Gustavo

1,231件の閲覧回数
dynamix
Contributor II

Great help! Thanks a lot

0 件の賞賛
返信