imxrt serial downloader issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imxrt serial downloader issue

ソリューションへジャンプ
799件の閲覧回数
ancymuhammed
Contributor III

We are using iMXRT1176 for one of our project. USB1 is used for OTG (Serial downloader) and device. Whether USB1_VBUS has to be connected to 5V inorder to work as serial downloader. 

Currently programming is successful only after connecting 5V to VBUS of iMXRT. Whether this connection is mandatory. 

0 件の賞賛
返信
1 解決策
785件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Yes, it should be connected. If USB1 is unused then you can leave unconnected USB1_DN, USB1_DP, USB1_VBUS.

Best regards,
Omar

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
786件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Yes, it should be connected. If USB1 is unused then you can leave unconnected USB1_DN, USB1_DP, USB1_VBUS.

Best regards,
Omar

0 件の賞賛
返信