imxRT1060 EVB SHARING PINS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imxRT1060 EVB SHARING PINS

1,075 次查看
giannigrondona
Contributor III

Hi

I have an imxrt1060 Evaluation board and in the schematic drawing there is a pin sharing between JTAG and ETH (ETH_RESET_N is shared with JTAG_TDI and ETH_INT is shared with JTAG_TDO) . Can I have problems if I use this configuration of pins to make a new card with the same micro?

Best Regards

Giovanni Grondona

标记 (1)
0 项奖励
回复
1 回复

820 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Giovanni Grondona,

You won't have any problems if you use this configuration. But, if you are planning to use JTAG to program/debug your i.MXRT and in your application you change the mode of the JTAG pins to ETH then you won't be able to debug your program. If you use SWD to program/debug your application (which is the case of the i.MXRT1060-EVK) then you won't have any problems with these pins.  

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复