iMXRT1064 with latest Emwin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMXRT1064 with latest Emwin

979件の閲覧回数
anujtanksali
Contributor II

Hello,

Am using iMXRT1064 controller and using Emwin for GUI. I came to know that Emwin ver 6.14 is released but could not find this library on NXP emwin web page. Can you please share the latest emwin ver 6.14. library for use with iMXRT1064 device.

I was able to download 6.10 libraries from NXP emwin web page but need ver 6.14 library

I plan to use Keyboard widget in my project and observed that this widget is added in Emwin ver 6.14. 

Thanks

Regards,

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

895件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi  Anuj Tanksali,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I'm afraid that the v6.14 is unavailable to download now. And you need to contact the Segger if you want to use the lasted version.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

895件の閲覧回数
anujtanksali
Contributor II

Hi jeremyzhou‌,

Thanks for the reply.

I wanted the emwin library file to use on iMXRT1064 device. As this is a NXP device i think it should be provided by NXP

I will check with segger but when will this be available from NXP. 

Regards,

Anuj

0 件の賞賛
返信