iMX RT GPIO / PAD / Peripherals

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX RT GPIO / PAD / Peripherals

1,448件の閲覧回数
mjbcswitzerland
Specialist V

Hi All

After working with the iMX RT 1020 for a short amount of time I have been rather surprised at the complexity of matching up GPIOs (which I believe most programmers 'think' in) with PADs (which the chip designers probably think in) and pin peripherals (which are related to both but rather muddled up). I also noted that the EVBs circuit diagram references pads and not even GPIOs on the chip!

In the data sheet and user's manual I don't find an overview of these so I have created a spread sheet to make life somewhat easier.

It is attached and I would like to know whether this is of interest / use to programmers and circuit designers? If not, please explain how you are working out these things from the manual alone ;-)

Regards

Mark

タグ(3)
2 返答(返信)

1,260件の閲覧回数
Yuri
NXP Employee
NXP Employee
0 件の賞賛
返信

1,260件の閲覧回数
mjbcswitzerland
Specialist V

Hi All

Since I need code that originates from various Kinetis development to run on i.MX RT parts without porting effort I have made a video of the solution finalised on here:

https://youtu.be/SmFTi8hlba0

Regards

Mark

uTasker - for Kinetis and i.MX RT compatibility....