i.mx RT1050: Boot from SPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx RT1050: Boot from SPI

1,746件の閲覧回数
christiangradl
Contributor III

Hi,
can i.mx RT1050 boot from a SPI Flash (e.g. Winbond W25N01GVZEIG)? Is this possible with FlexSPI?

ラベル(1)
4 返答(返信)

1,289件の閲覧回数
jay_heng
NXP Employee
NXP Employee

You can also try this tool, with this tool, You can flash bare image into various boot devices easily and don't need to care about headers (ivt, boot data...)

GitHub - JayHeng/nxp-sec-boot-ui: A one-stop GUI tool to work with NXP MCU (Kinetis, i.MXRT, LPC) RO... 

0 件の賞賛
返信

1,289件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Could You provide more detailed description of the nxp-sec-boot-ui in English

(only introduction is available now)?

Regards,

Yuri.

0 件の賞賛
返信

1,289件の閲覧回数
jay_heng
NXP Employee
NXP Employee

Hi Yuri,

  English version user guide is available now.

Best Regards,

Jay

1,289件の閲覧回数
art
NXP Employee
NXP Employee

Q. Can i.mx RT1050 boot from a SPI Flash (e.g. Winbond W25N01GVZEIG)?

A. Yes, it can.

Q. Is this possible with FlexSPI?

A. Yes, it is possible.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信