i.MXRT1050 EVK - SDRAM support with Zephyr

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT1050 EVK - SDRAM support with Zephyr

Jump to solution
1,748 Views
treto
Contributor I

Hi,

I'm using the i.MXRT1050 EVK with Zephyr RTOS. I'm running into an issue with my data size as I need a relatively large frame buffer that won't fit inside the internal SRAM.

Is there support (or a plan) to support SDRAM with Zephyr RTOS?

Best regards,

Lukasz

Tags (1)
0 Kudos
Reply
1 Solution
1,496 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Lukas,

As mentioned we do not yet support RT1050 SDRAM in Zephyr. The immediate goal is to enable the Hyperflash, and after that SDRAM will be scheduled but I’m not sure of the timeline yet.

Since Zephyr is an open source project like Linux, customers can contribute features if they need them sooner. There is also support available through the Zephyr community on the public mailing lists.

https://www.zephyrproject.org/developers/how-to-contribute/


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,497 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Lukas,

As mentioned we do not yet support RT1050 SDRAM in Zephyr. The immediate goal is to enable the Hyperflash, and after that SDRAM will be scheduled but I’m not sure of the timeline yet.

Since Zephyr is an open source project like Linux, customers can contribute features if they need them sooner. There is also support available through the Zephyr community on the public mailing lists.

https://www.zephyrproject.org/developers/how-to-contribute/


Regards,
Carlos
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,496 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Lukas,

to my knowledge there are no plans. But I will check and if I find something I will let you know.

Regards,

Carlos

0 Kudos
Reply