elftosb signing certificate location issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

elftosb signing certificate location issue

1,104件の閲覧回数
anooppk
Contributor I

Hello,

    In my project, I am using elftosb and cst tool to create signed binary and I am trying to read the signing certificate from an external pen drive. if I give the whole path of the signing certificate as mentioned below, elftosb generating syntax error

anooppk_0-1640838846910.png

command.db file

I am storing the certificate in external usb. SRK table file stored in the same directory of elftosb

anooppk_1-1640839109253.png

error while running elftosb

 

Is mandatory to store the certificate in the same folder of elftosb?

 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,076件の閲覧回数
anooppk
Contributor I

Is there any way to give an absolute address in db  to locate the .pem file, because we want to read the certificate from an external USB.

0 件の賞賛
返信

1,091件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is mandatory to store the certificate in the same folder of elftosb?
-- Yes, as the bd file provide the relative address instead of the absolute address for locating the pem file
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,072件の閲覧回数
anooppk
Contributor I

Is there any way to give an absolute address in db to locate the .pem file, because we want to read the certificate from an external USB?

0 件の賞賛
返信