blhost cannot establish a connection based on the USB path

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

blhost cannot establish a connection based on the USB path

600件の閲覧回数
Vinos
Contributor III

Since I want to simultaneously connect multiple RT1170 USB devices to a single computer for concurrent production, using blhost requires connecting via USB path.

The relevant connection examples can be found on page 10 of the document below

https://www.nxp.com/docs/en/user-guide/MCUBLHOSTUG.pdf 

 

However, even after querying the USB path through this step, I still cannot establish a connection successfully.

Prompt as shown in the following image. How can I establish a connection through the USB path?

1.png

 

 

0 件の賞賛
返信
1 返信

594件の閲覧回数
Vinos
Contributor III

After my test, it is possible to connect to the device in this way, but it is necessary to try sending commands multiple times before the command finally returns success.

Why is there a high probability of command execution failure?

0 件の賞賛
返信