about imx.rt1052 USB example of USB_ device_ msc_ Sdcard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about imx.rt1052 USB example of USB_ device_ msc_ Sdcard

1,063 Views
944706426
Contributor III

 this example can read all the space of SD card through USB by default. If I want to set the last 1g capacity of SD card to be recognized and used by the computer, I don't know where to change it. Please let me know. Thank you.

Labels (1)
0 Kudos
Reply
1 Reply

987 Views
jeremyzhou
NXP Employee
NXP Employee

Hi ,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Regarding your purpose, you should adapt these event handles actions: kUSB_DeviceMscEventReadCapacity, kUSB_DeviceMscEventWriteResponse, kUSB_DeviceMscEventWriteRequest, kUSB_DeviceMscEventReadRequest in the USB_DeviceMscCallback.
Hope this is clear.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply