GPIO_init();
LPUART2_init();
while(1)
{
IOMUXC_SetPinMux(IOMUXC_GPIO_AD_B1_02_GPIO1_IO18, 0U);
GPIO_WritePinOutput(GPIO1, 18U, 0);
use_tmr_delay1ms();
GPIO_WritePinOutput(GPIO1, 18U, 1);
IOMUXC_SetPinMux(IOMUXC_GPIO_AD_B1_02_LPUART2_TX, 0U);
LPUART_Send(0x55);
}
Sometimes it's normal like this:
normal
But sometimes it's not normal,it should have some high level before start bit
error
Hello
Hope you are well.
It is important to add the pin configuration when you change between LPUART and GPIO.
The time that pin stays in high from GPIO_Write to LPUART_Send is variable, if you want to keep it consistent I suggest you add a small delay between.
If you have more questions do not hesitate to ask me.
Best regards,
Omar