Silicon Rev on RT1062

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Silicon Rev on RT1062

1,000 Views
tpetrovic
Contributor I

The final character in the RT1062 part number specifies the Silicon Rev. It is either A for silicon rev A0, or B for silicon rev A1. What is the difference between these two revisions? Are they hardware and source code compatible?

 

0 Kudos
Reply
1 Reply

990 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

For RT1060/RT1064 revA1, we fixed a USB isochronous errata that only impacts a very limited number of use cases. Primarily in audio application.  The errata shows up when the RT is used in USB isochronous mode, plugged into a hub, with multiple devices plugged into the hub and the devices have the same endpoint number. Very limited use case. 
 
Both revisions are software and hardware compatible with each other.
 
Regards,
Victor 
0 Kudos
Reply