SEMC Serial NAND

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SEMC Serial NAND

1,280 Views
Ankush_9881
Contributor II

Hello All,

 I am working with iMXRT1176, I have one query like, Is it possible to interface Serial SLC NAND flash via SEMC1 and boot the MCU ?

Also with above configuration , is it possible to use SDRAM and SLC NAND Flash on SEMC ?

(example: NAND Flash MX35LFxGE4AB) 

0 Kudos
Reply
2 Replies

856 Views
maouncle
Contributor I

Can you recommand one type nand device for iMXRT1176?

0 Kudos
Reply

1,259 Views
jay_heng
NXP Employee
NXP Employee

SEMC can only work with Raw NAND (ONFI 1.0), you can use FlexSPI to interface Serial (SPI) NAND (JESD216).

it is possible to use SDRAM and Raw NAND Flash on SEMC

0 Kudos
Reply