RT101X USB FS/HS device without external crystal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT101X USB FS/HS device without external crystal

Jump to solution
1,081 Views
jh0
Contributor IV

Does RT101X can work as FS or / and HS USB device (not host) without using external crystal?

Regards,

JH

0 Kudos
Reply
1 Solution
1,075 Views
jay_heng
NXP Employee
NXP Employee

External 24MHz crystal is necessary for USB application (PHY should be driven by 480MHz clk). as internal RC24M (maximum 20% accuracy error) is only for low speed peripherals

View solution in original post

1 Reply
1,076 Views
jay_heng
NXP Employee
NXP Employee

External 24MHz crystal is necessary for USB application (PHY should be driven by 480MHz clk). as internal RC24M (maximum 20% accuracy error) is only for low speed peripherals