RT 1062 PWM and UART Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RT 1062 PWM and UART Problem

跳至解决方案
675 次查看
EthanKu
Contributor I
  1. if PWM module is used for the input function , do we select whether an PWM module includes a timer or not ? and what is different on PWM module with /without a timer?

 

EthanKu_0-1661763214476.png

2. do UART have a SWAP SW setting by TX and RX if a wrong connection occurs 

标记 (1)
0 项奖励
回复
1 解答
659 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @EthanKu ,

   You are welcome!

   If your question is solved, please help me to mark the correct answer, just to close this case.

   Any new issues, welcome to create the new question post!

Best Regards,

kerry

在原帖中查看解决方案

0 项奖励
回复
3 回复数
669 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @EthanKu 

   Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

Answer your questions:

1. if PWM module is used for the input function , do we select whether an PWM module includes a timer or not ? and what is different on PWM module with /without a timer?

=>Answer: If you select the pin as the PWM function, it is not the TMR pin.

As you know, PWM and TMR is totally the different peripheral module.

So, if you select it as the PWM in pinmux, then it is the PWM pin.

 

2. Do UART have a SWAP SW setting by TX and RX if a wrong connection occurs 

=>Answer: UART no SWAP function, you can check the UART pin, TX and RX is not shared, so, you need to make sure HW connection is correct.

 

Wish it helps you!

Best Regards,

kerry

 

 

0 项奖励
回复
662 次查看
EthanKu
Contributor I

HI Kerry 

OK , i got it 

thanks 

0 项奖励
回复
660 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @EthanKu ,

   You are welcome!

   If your question is solved, please help me to mark the correct answer, just to close this case.

   Any new issues, welcome to create the new question post!

Best Regards,

kerry

0 项奖励
回复