OM13790 USB C Shield SDK Documentation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OM13790 USB C Shield SDK Documentation

816 次查看
benolayinka
Contributor III

Im using the OM13790 shield to see how difficult it would be to add usb-c pd and negotiation to an existing IMX1050RT project.

I've managed to download the SDK and I see some examples, but is there any documentation anywhere for the SDK?

The example code is a mess of if defs and there's no API information, not even a comment about how to use anything.

The SDK is really just a usb->pd folder with what I guess are PD negotiation drivers. What about configuring DFP/UFP? What about an I2C API?

I hope I'm just not finding the documentation.. because it seems crazy to sell this device as a revolutionary 'plug and play' solution but offer absolutely no documentation.. I'm going to spend forever trying to reverse engineer the examples, it looks like

标记 (2)
0 项奖励
回复
1 回复

766 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Sorry for the later reply.

If you download the SDK package with OM13790HOST?

pastedImage_3.png

pastedImage_2.png

During SDK package download, you can also download related documents:

pastedImage_1.png

After SDK Documentation dowloaded, you could find two files for MCUXpresso SDK USB Type-C PD Stack:

pastedImage_4.png

Wish it helps.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复