MIMXRT1170-EVK bricked

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MIMXRT1170-EVK bricked

1,304 次查看
daniJVV
Contributor II

I've been using this board for a month, but trying a new software it got bricked. 

When I try to upload a working project this is the result:

daniJVV_1-1680618721802.png

 

I readed about MCU boot utility, but when I try access to the board the USB is not found, and shows this error:

daniJVV_0-1680618681685.png

Then I put the board in Serial downloader and I can upload the firmware, but this is not working.

With the Serial downloader and MCU boot utility I have this message:

daniJVV_2-1680618883502.png

I need to unlock this to continue working. Does anyone knows what is happening?

Thank you in advance.

0 项奖励
回复
4 回复数

1,290 次查看
RaRo
NXP TechSupport
NXP TechSupport

Hello @daniJVV ,

Could you please change the MCU Device in MCU Boot Utility to i.MXRT117x and try again?

RaulRomero_0-1680630668654.png

[MCU Boot Utility's Target Setup]

Let us know if you have another issue.

Best regards, Raul.

0 项奖励
回复

1,226 次查看
daniJVV
Contributor II

Hi @RaRo 

I tried to debug a touch screen example that was working before this problem, and now there is no errors when uploading the firmware.

But the problem with USB-HID MCU Boot Utility continues.

 

Daniel Prieto

 

0 项奖励
回复

1,237 次查看
daniJVV
Contributor II

Hello @RaRo 

I got this message when I tried to connect with USB:

daniJVV_0-1681196393690.png

With UART I can connect, but I don't know which parameters to look at.
Is there something to check in any memory (boot image, eFuse...)?

daniJVV_1-1681198113941.png

Thank you for your help.

0 项奖励
回复

1,210 次查看
RaRo
NXP TechSupport
NXP TechSupport

Hello @daniJVV,

Could you please try with the following steps?

  • First, move your SW1 to 0001 (Serial Downloader mode).
  • Secondly, place a jumper in position 5-6 in J38 to power the board trough J11.
  • Then, connect both J11 and J20 to your computer and open the NXP MCU Boot Utility.
  • After that, select the i.MXRT117x as your MCU Device.
  • Connect to ROM trough UART.
  • Then, check now if is detecting your USB-HID connection. Turn off the board and change the position of the jumper in J38 to position 3-4.
  • Finally, power up the board again only through J20, and check if your board is being detected.

RaulRomero_0-1681247772892.png

[Testing configuration in a MIMXRT1170-EVK board]

Best regards, Raul.

0 项奖励
回复