MDIO hold time adjustment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MDIO hold time adjustment

Jump to solution
736 Views
Eugene3
Contributor II

Hi

I'm evaluating RT1170 on my board.

I connect RT1170 and ethernet phy by SMI. As far as I checked SMI waveform, the hold time of MDIO is not enough about 8ns when RT1170 outputs. 

I'd like to change the hold time more than 10ns. 

Could you tell me how to change the hold time of MDIO?

 

This is the spec of my phy device. T4.3 should be more than 10ns.

Eugene3_1-1706572604808.png

 

0 Kudos
Reply
1 Solution
689 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

Thank you for contacting NXP support.

The 10 ns is the minimum hold time on the MDIO output. In relation with the bus frequency this setting may be increased. This field description to change this is given on the Chapter 60.5.1.8.4 of the reference manual on the table of Hold Time.

By changing this configuration you van increase the hold time.

nxf77486_0-1706655104617.png

 

View solution in original post

0 Kudos
Reply
1 Reply
690 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

Thank you for contacting NXP support.

The 10 ns is the minimum hold time on the MDIO output. In relation with the bus frequency this setting may be increased. This field description to change this is given on the Chapter 60.5.1.8.4 of the reference manual on the table of Hold Time.

By changing this configuration you van increase the hold time.

nxf77486_0-1706655104617.png

 

0 Kudos
Reply