On Page 1050 of IMCRT1010RM.pdf TCR2
NOTE: Depending on the device, some Master Clock options might not be available. See the chip- specific information for the meaning of each option.
MSEL
00b - Bus Clock selected.
01b - Master Clock (MCLK) 1 option selected.
10b - Master Clock (MCLK) 2 option selected.
11b - Master Clock (MCLK) 3 option selected.
Which option to use?
To select an external MCLK which option?
To select S/PDIF RX recovered MCLK as MCLK for the SAI which option?
Please help to clarify.
Many thanks.
emag
Hi Emag,
You can see MCLK mux options in Figure 31-3. Audio subsystem clocking diagram. Additionally, you can use MCUXpresso Config Tools to configure this directly.
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------