How to enter SEMC SDRAM into low power
09-27-2024
06:06 PM
330件の閲覧回数
rjengr
Contributor I
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
We are using a imxrt106F, with VDD_HIGH_IN, SNVS_IN, and DCDC_IN tied together. However the issue we see is entering into SNVS does not automatically put the SDRAM into low power mode as our SDRAM is constantly powered. We are seeing very high power consumption. How can we put the SDRAM into low power mode?
1 返信
10-02-2024
11:37 AM
291件の閲覧回数


NXP TechSupport
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
If the SDRAM has a low power mode then you need to enter the command to send it to low power before setting the mcu at SNVS mode.
Ideally, SDRAM is powered-off on SNVS mode since external DC/DC(which powers SDRAM) is turned off.
Best regards,
Omar