EVK-MIMXRT685: I3C examples

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EVK-MIMXRT685: I3C examples

ソリューションへジャンプ
1,933件の閲覧回数
bslava
Contributor II

Hello,

I am interested in the I3C development platform and for this I was going to order the EVK-MIMXRT685, but before that I checked the examples supplied with that platform. Unfortunately for me, unlike I2C, I2S, USART, etc., where 3 types of technologies are supported: polling, interrupt and DMA, the I3C folder contains only example for polling. Does this mean that the implementation of this IP does not support interrupts and DMA?

And another question about the documentation. I cannot find a detailed description of the RT600 microcontroller. The only existing document does not contain documentation on peripherals and their registers. Did I miss something?

Thanks.

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,927件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Bslava,

Please refer to the User Manual (link below), which covers the modules and its registers in more detail.

https://www.nxp.com/docs/en/user-guide/UM11147.pdf

For the rest of the i.MXRT600 documentation please refer to the following link:

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/i-mx-rt-crossover-...

As for the examples available on the SDK, these may vary from module to module so not all scenarios are always present as an example project. My apologies for the inconvenience.

I hope that this information helps!

Regards,
Gustavo

元の投稿で解決策を見る

2 返答(返信)
1,928件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Bslava,

Please refer to the User Manual (link below), which covers the modules and its registers in more detail.

https://www.nxp.com/docs/en/user-guide/UM11147.pdf

For the rest of the i.MXRT600 documentation please refer to the following link:

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/i-mx-rt-crossover-...

As for the examples available on the SDK, these may vary from module to module so not all scenarios are always present as an example project. My apologies for the inconvenience.

I hope that this information helps!

Regards,
Gustavo

1,913件の閲覧回数
bslava
Contributor II

Gustavo,

Thank you very much!

Slava

0 件の賞賛
返信