Difference between LPSPI, Flexcomm SPI, and traditional SPI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Difference between LPSPI, Flexcomm SPI, and traditional SPI

跳至解决方案
264 次查看
MichaelC_Future
Contributor II

@Pablo_Ramos Will you please clarify difference (speed/frequency, voltages, current consumption, etc.) between LPSPI, Flexcomm SPI, and traditional SPI specifically running on i.MX RT 1170 EVK. 

0 项奖励
回复
1 解答
221 次查看
Pablo_Ramos
NXP Employee
NXP Employee

Hi @MichaelC_Future ,

RT1170 can perform SPI interface with LPSPI and FlexIO modules. Flexcomm SPI and traditional SPI are not supported for such device.

For voltages and currents please refer to the 4.3.1.2 General purpose I/O (GPIO) DC parameters section from datasheet.

Regarding frequency LPSPI has a maximum frequency of 30MHz. For more information, please refer to the Chapter 4.9.1 LPSPI timing parameters section from datasheet.

Regarding the FlexIO module it has a maximum baud rate in SPI Master mode of FlexIO clock frequency / 4 and in SPI Slave mode of FlexIO clock frequency / 6 (this due to synchronization delays). For more information, please refer to the Chapter 67 from reference manual.

For power consumption there is no specification of how much each module consume on RT1170, but customer can test this by checking the difference of consumption with the module on and off. An apology for the inconvenience.

Hope it helps you!

在原帖中查看解决方案

2 回复数
222 次查看
Pablo_Ramos
NXP Employee
NXP Employee

Hi @MichaelC_Future ,

RT1170 can perform SPI interface with LPSPI and FlexIO modules. Flexcomm SPI and traditional SPI are not supported for such device.

For voltages and currents please refer to the 4.3.1.2 General purpose I/O (GPIO) DC parameters section from datasheet.

Regarding frequency LPSPI has a maximum frequency of 30MHz. For more information, please refer to the Chapter 4.9.1 LPSPI timing parameters section from datasheet.

Regarding the FlexIO module it has a maximum baud rate in SPI Master mode of FlexIO clock frequency / 4 and in SPI Slave mode of FlexIO clock frequency / 6 (this due to synchronization delays). For more information, please refer to the Chapter 67 from reference manual.

For power consumption there is no specification of how much each module consume on RT1170, but customer can test this by checking the difference of consumption with the module on and off. An apology for the inconvenience.

Hope it helps you!

205 次查看
MichaelC_Future
Contributor II

Hi @Pablo_Ramos,

 

This is great information! Thank you for your help!

0 项奖励
回复