About IMXRT1010 RAM available

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About IMXRT1010 RAM available

202 次查看
LuigiV
Contributor III

I'm using the IMXRT1010 EVM to develop a convolution project and I need to have available the maximum size of RAM; compiling and linking my FW I get this error:

"

10:07:50 **** Incremental Build of configuration Debug for project evkmimxrt1010_sai_interrupt_record_playback ****

make -r -j4 all

Building target: evkmimxrt1010_sai_interrupt_record_playback.axf

Invoking: MCU Linker

arm-none-eabi-gcc -nostdlib -Xlinker -no-warn-rwx-segments -Xlinker -Map="evkmimxrt1010_sai_interrupt_record_playback.map" -Xlinker --gc-sections -Xlinker -print-memory-usage -Xlinker --sort-section=alignment -Xlinker --cref -mcpu=cortex-m7 -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -T evkmimxrt1010_sai_interrupt_record_playback_Debug.ld -o "evkmimxrt1010_sai_interrupt_record_playback.axf" ./xip/evkmimxrt1010_flexspi_nor_config.o ./xip/fsl_flexspi_nor_boot.o ./utilities/fsl_assert.o ./utilities/fsl_debug_console.o ./utilities/fsl_memcpy.o ./utilities/fsl_str.o ./startup/startup_mimxrt1011.o ./source/MathRoutines.o ./source/sai_interrupt_record_playback.o ./source/semihost_hardfault.o ./drivers/fsl_clock.o ./drivers/fsl_common.o ./drivers/fsl_common_arm.o ./drivers/fsl_gpio.o ./drivers/fsl_lpi2c.o ./drivers/fsl_lpuart.o ./drivers/fsl_sai.o ./device/system_MIMXRT1011.o ./component/uart/fsl_adapter_lpuart.o ./component/lists/fsl_component_generic_list.o ./component/i2c/fsl_adapter_lpi2c.o ./codec/port/wm8960/fsl_codec_wm8960_adapter.o ./codec/fsl_codec_common.o ./codec/fsl_codec_i2c.o ./codec/fsl_wm8960.o ./board/board.o ./board/clock_config.o ./board/pin_mux.o ./CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_q15.o ./CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_q7.o ./CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_s8.o ./CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_u8.o ./CMSIS/NN/Source/SoftmaxFunctions/arm_softmax_with_batch_q7.o ./CMSIS/NN/Source/SVDFunctions/arm_svdf_s8.o ./CMSIS/NN/Source/ReshapeFunctions/arm_reshape_s8.o ./CMSIS/NN/Source/PoolingFunctions/arm_avgpool_s8.o ./CMSIS/NN/Source/PoolingFunctions/arm_max_pool_s8.o ./CMSIS/NN/Source/PoolingFunctions/arm_pool_q7_HWC.o ./CMSIS/NN/Source/NNSupportFunctions/arm_nn_accumulate_q7_to_q15.o ./CMSIS/NN/Source/NNSupportFunctions/arm_nn_add_q7.o ./CMSIS/NN/Source/NNSupportFunctions/arm_nn_depthwise_conv_nt_t_padded_s8.o ./CMSIS/NN/Source/NNSupportFunctions/arm_nn_depthwise_conv_nt_t_s8.o ./CMSIS/NN/Source/NNSupportFunctions/arm_nn_mat_mul_core_1x_s8.o ./CMSIS/NN/Source/NNSupportFunctions/arm_nn_mat_mul_core_4x_s8.o ./CMSIS/NN/Source/NNSupportFunctions/arm_nn_mat_mult_nt_t_s8.o ./CMSIS/NN/Source/NNSupportFunctions/arm_nn_mult_q15.o ./CMSIS/NN/Source/NNSupportFunctions/arm_nn_mult_q7.o ./CMSIS/NN/Source/NNSupportFunctions/arm_nn_vec_mat_mult_t_s8.o ./CMSIS/NN/Source/NNSupportFunctions/arm_nn_vec_mat_mult_t_svdf_s8.o ./CMSIS/NN/Source/NNSupportFunctions/arm_nntables.o ./CMSIS/NN/Source/NNSupportFunctions/arm_q7_to_q15_no_shift.o ./CMSIS/NN/Source/NNSupportFunctions/arm_q7_to_q15_reordered_no_shift.o ./CMSIS/NN/Source/NNSupportFunctions/arm_q7_to_q15_reordered_with_offset.o ./CMSIS/NN/Source/NNSupportFunctions/arm_q7_to_q15_with_offset.o ./CMSIS/NN/Source/FullyConnectedFunctions/arm_fully_connected_mat_q7_vec_q15.o ./CMSIS/NN/Source/FullyConnectedFunctions/arm_fully_connected_mat_q7_vec_q15_opt.o ./CMSIS/NN/Source/FullyConnectedFunctions/arm_fully_connected_q15.o ./CMSIS/NN/Source/FullyConnectedFunctions/arm_fully_connected_q15_opt.o ./CMSIS/NN/Source/FullyConnectedFunctions/arm_fully_connected_q7.o ./CMSIS/NN/Source/FullyConnectedFunctions/arm_fully_connected_q7_opt.o ./CMSIS/NN/Source/FullyConnectedFunctions/arm_fully_connected_s8.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_1_x_n_s8.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_1x1_HWC_q7_fast_nonsquare.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_1x1_s8_fast.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_HWC_q15_basic.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_HWC_q15_fast.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_HWC_q15_fast_nonsquare.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_HWC_q7_RGB.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_HWC_q7_basic.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_HWC_q7_basic_nonsquare.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_HWC_q7_fast.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_HWC_q7_fast_nonsquare.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_s8.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_convolve_wrapper_s8.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_depthwise_conv_3x3_s8.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_depthwise_conv_s8.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_depthwise_conv_s8_opt.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_depthwise_conv_u8_basic_ver1.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_depthwise_conv_wrapper_s8.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_depthwise_separable_conv_HWC_q7.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_depthwise_separable_conv_HWC_q7_nonsquare.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_nn_depthwise_conv_s8_core.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_nn_mat_mult_kernel_q7_q15.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_nn_mat_mult_kernel_q7_q15_reordered.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_nn_mat_mult_kernel_s8_s16.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_nn_mat_mult_kernel_s8_s16_reordered.o ./CMSIS/NN/Source/ConvolutionFunctions/arm_nn_mat_mult_s8.o ./CMSIS/NN/Source/ConcatenationFunctions/arm_concatenation_s8_w.o ./CMSIS/NN/Source/ConcatenationFunctions/arm_concatenation_s8_x.o ./CMSIS/NN/Source/ConcatenationFunctions/arm_concatenation_s8_y.o ./CMSIS/NN/Source/ConcatenationFunctions/arm_concatenation_s8_z.o ./CMSIS/NN/Source/BasicMathFunctions/arm_elementwise_add_s8.o ./CMSIS/NN/Source/BasicMathFunctions/arm_elementwise_mul_s8.o ./CMSIS/NN/Source/ActivationFunctions/arm_nn_activations_q15.o ./CMSIS/NN/Source/ActivationFunctions/arm_nn_activations_q7.o ./CMSIS/NN/Source/ActivationFunctions/arm_relu6_s8.o ./CMSIS/NN/Source/ActivationFunctions/arm_relu_q15.o ./CMSIS/NN/Source/ActivationFunctions/arm_relu_q7.o ./CMSIS/DSP/Source/TransformFunctions/TransformFunctions.o ./CMSIS/DSP/Source/TransformFunctions/TransformFunctionsF16.o ./CMSIS/DSP/Source/SupportFunctions/SupportFunctions.o ./CMSIS/DSP/Source/SupportFunctions/SupportFunctionsF16.o ./CMSIS/DSP/Source/StatisticsFunctions/StatisticsFunctions.o ./CMSIS/DSP/Source/StatisticsFunctions/StatisticsFunctionsF16.o ./CMSIS/DSP/Source/SVMFunctions/SVMFunctions.o ./CMSIS/DSP/Source/SVMFunctions/SVMFunctionsF16.o ./CMSIS/DSP/Source/QuaternionMathFunctions/QuaternionMathFunctions.o ./CMSIS/DSP/Source/MatrixFunctions/MatrixFunctions.o ./CMSIS/DSP/Source/MatrixFunctions/MatrixFunctionsF16.o ./CMSIS/DSP/Source/InterpolationFunctions/InterpolationFunctions.o ./CMSIS/DSP/Source/InterpolationFunctions/InterpolationFunctionsF16.o ./CMSIS/DSP/Source/FilteringFunctions/FilteringFunctions.o ./CMSIS/DSP/Source/FilteringFunctions/FilteringFunctionsF16.o ./CMSIS/DSP/Source/FastMathFunctions/FastMathFunctions.o ./CMSIS/DSP/Source/FastMathFunctions/FastMathFunctionsF16.o ./CMSIS/DSP/Source/DistanceFunctions/DistanceFunctions.o ./CMSIS/DSP/Source/DistanceFunctions/DistanceFunctionsF16.o ./CMSIS/DSP/Source/ControllerFunctions/ControllerFunctions.o ./CMSIS/DSP/Source/ComplexMathFunctions/ComplexMathFunctions.o ./CMSIS/DSP/Source/ComplexMathFunctions/ComplexMathFunctionsF16.o ./CMSIS/DSP/Source/CommonTables/CommonTables.o ./CMSIS/DSP/Source/CommonTables/CommonTablesF16.o ./CMSIS/DSP/Source/BayesFunctions/BayesFunctions.o ./CMSIS/DSP/Source/BayesFunctions/BayesFunctionsF16.o ./CMSIS/DSP/Source/BasicMathFunctions/BasicMathFunctions.o ./CMSIS/DSP/Source/BasicMathFunctions/BasicMathFunctionsF16.o

c:/nxp/mcuxpressoide_11.8.1_1197/ide/plugins/com.nxp.mcuxpresso.tools.win32_11.8.1.202308071233/tools/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: evkmimxrt1010_sai_interrupt_record_playback.axf section `.bss' will not fit in region `SRAM_ITC'

c:/nxp/mcuxpressoide_11.8.1_1197/ide/plugins/com.nxp.mcuxpresso.tools.win32_11.8.1.202308071233/tools/bin/../lib/gcc/arm-none-eabi/12.2.1/../../../../arm-none-eabi/bin/ld.exe: region `SRAM_ITC' overflowed by 5108 bytes

Memory region Used Size Region Size %age Used

BOARD_FLASH: 57432 B 16 MB 0.34%

SRAM_ITC: 37876 B 32 KB 115.59%

SRAM_DTC: 2 KB 32 KB 6.25%

SRAM_OC: 0 GB 64 KB 0.00%

NCACHE_REGION: 0 GB 0 GB

collect2.exe: error: ld returned 1 exit status

make[1]: *** [makefile:80: evkmimxrt1010_sai_interrupt_record_playback.axf] Error 1

make: *** [makefile:71: all] Error 2

"make -r -j4 all" terminated with exit code 2. Build might be incomplete.

 

10:07:51 Build Failed. 4 errors, 0 warnings. (took 1s.94ms)

"

Only the SRAM_ITC is used for data, is there a way to set the environment to have all the SRAM (DTC and OC) available for data ?

 

Thank you

 

Luigi

0 项奖励
回复
1 回复

180 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @LuigiV ,

  To your situation, it is easy to resolve, mainly 2 ways:

1. define your related variable to the DTCM or the OCRAM.

You can refer to this document:

https://community.nxp.com/docs/DOC-335283

: Use the keyword “__attribute__”

2. Reallocate your flexRAM, to make your ITCM size larger.

More details, you can refer to this application note:

https://www.nxp.com/docs/en/application-note/AN12077.pdf

You also can refer to my document:

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/The-RT-speech-recognition-system-based-on-VIT-to...

chapter 5.2 VIT LWIP merger memory is not enough

 

Wish it helps you!

If you still have question about it, please kindly let me know.

If your question is solved, please help me to mark the correct answer, just to close this case.

Any new issues, welcome to create the new question post, thanks.

Best Regards,

Kerry

0 项奖励
回复