1064 with dual-die package (128Mbit) HyperRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1064 with dual-die package (128Mbit) HyperRAM

Jump to solution
1,755 Views
p_shep
Contributor IV

It's my favourite subject... again!

So we're having trouble sourcing enough of the Cypress S27KS0642GABHI02 for our project and have a couple of Winbond parts to try:

W956D8MBYA5I (on the 'tested' list in AN12239)

W957D8MFYA5I (16Mbyte dual-die package)

Now the 'tested' winbond one is failing a memtest after a few mins when using the same settings as the original Cypress. I guess a timing issue somewhere? Funnily enough it fails immediately at lower clocks rates.

On the DDP Winbond, the memtest fails at the 8Mb boundary, but it appears that the memory after can be read - at least with the memory viewer. Is there a way to get the FlexSPI driver to cope with the dual-die arrangement? If the size is set to just 8Mbytes, the memtest seems to be working fine with the Cypress settings.

Labels (1)
0 Kudos
Reply
1 Solution
1,751 Views
p_shep
Contributor IV

So setting:

config.ahbConfig.enableAHBPrefetch = false;

Will get it working. But that's surely going to be a BIG hit on performance?

View solution in original post

0 Kudos
Reply
3 Replies
1,751 Views
p_shep
Contributor IV

Just found this:

https://community.nxp.com/t5/i-MX-RT/I-MX-RT1176-use-128Mb-Hyper-Ram-has-Problem-when-enable-prefetc...

So MPU has the area set as device, and I've created 2 linker sections to cover the area, but still not working

0 Kudos
Reply
1,752 Views
p_shep
Contributor IV

So setting:

config.ahbConfig.enableAHBPrefetch = false;

Will get it working. But that's surely going to be a BIG hit on performance?

0 Kudos
Reply
1,733 Views
p_shep
Contributor IV

Yep, turning prefetch off has a dramatic affect on performance..

At 327MHz, my memtest goes from ~1140ms to 1884ms to complete.

 

So, ways to abort the prefetch at the 8Mb boundary?

0 Kudos
Reply