wifi in warp7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

wifi in warp7

Jump to solution
4,321 Views
dharmeshkanzari
Contributor II

hello there

can anyone tell me how to enable wifi in warp7??

Labels (1)
1 Solution
3,265 Views
daiane_angolini
NXP Employee
NXP Employee

Have you tried the procedure from WaRP7-User-Guide/Use_Cases.adoc at master · WaRP7/WaRP7-User-Guide · GitHub  already?

You are not going to ping google.com directly, you need to make sure you have configured a DNS server and you have Internet connection. At first, try to ping your local PC IP instead of an external DNS.

View solution in original post

0 Kudos
30 Replies
2,551 Views
dharmeshkanzari
Contributor II

ok thanks .

i tried to make yocto project image . i followed this link Warp7 Yocto : Part1 : setup, configure and gene... | element14 | WaRP7 .but i am getting error 

i got this link. FSL Community BSP . they said they have made yocto images.can you tell me from this link which image should i download??

0 Kudos
2,550 Views
daiane_angolini
NXP Employee
NXP Employee

dharmeshkanzariya‌, can you, please share what you have already tried? What is the kernel version you are using?

Artur is right, the WaRP7 community is being maintained in this site WaRP7 - The Next Generation IoT and Wearable De... | element14 | Design Center 

0 Kudos
2,550 Views
dharmeshkanzari
Contributor II

hi my kernel version is 

4.1.15-gc45e62f-dirty
#6 SMP PREEMPT Tue Jul 12 14:44:15 CST 2016.

i have tried  nano /etc/wpa_supplicant.conf

ctrl_interface=/var/run/wpa_supplicant
ctrl_interface_group=0
update_config=1
network={
ssid="abc"
scan_ssid=1
psk="87654321"
priority=5
}

my laptop is connected to wifi name "abc" and my password is 87654321.

after that i tried ping google.com. but it didn't work

0 Kudos
3,266 Views
daiane_angolini
NXP Employee
NXP Employee

Have you tried the procedure from WaRP7-User-Guide/Use_Cases.adoc at master · WaRP7/WaRP7-User-Guide · GitHub  already?

You are not going to ping google.com directly, you need to make sure you have configured a DNS server and you have Internet connection. At first, try to ping your local PC IP instead of an external DNS.

0 Kudos
2,550 Views
dharmeshkanzari
Contributor II

hi when i run this command i get this error.

root@imx7dwarp7:~# ifconfig wlan0 up
ifconfig: SIOCGIFFLAGS: No such device

is yocto image is necessary??

0 Kudos
2,550 Views
daiane_angolini
NXP Employee
NXP Employee

No, it's not. But you have to install the wifi module properly.

You can also try buildroot, master supports warp7

0 Kudos
2,550 Views
dharmeshkanzari
Contributor II

hi thanks . but i followed steps as you described

and  how to buildroot in warp 7??

0 Kudos
2,550 Views
daiane_angolini
NXP Employee
NXP Employee

The instructions from the User Guide use the yocto project image which includes the wifi firmware, the wifi driver modules, and wpa-supplicant package. You can use any rootfs if you know those pieces are included in the rootfs, it does not need to be yocto or buildroot. However, I really recommend you use or yocto or buildroot as we know they are working.

0 Kudos
2,550 Views
dharmeshkanzari
Contributor II

waiting for your response

0 Kudos
2,550 Views
daiane_angolini
NXP Employee
NXP Employee

I'm sorry for my delay. I was busy with unexpected interruptions.

You can download fsl-image-machine-test, last time I tested it included the wifi firmware properly.

0 Kudos
2,548 Views
dharmeshkanzari
Contributor II

hey thanks for your support.

i have downloaded  FSL Community BSP 2.2       xwayland

fsl-image-machine-test-imx7s-warp-20161124-6.rootfs.sdcard.gz
can you tell me how to update image into warp7
0 Kudos
2,550 Views
daiane_angolini
NXP Employee
NXP Employee

Please, take a look on User Guide, there is instructions to update yocto image, only u-boot, only kernel. A lot of tutorials.

And please, if you find any issue, please create an issue in the github so we can detail it.

GitHub - WaRP7/WaRP7-User-Guide: WaRP7 User Guide Source. For binary releases go to the release tab 

0 Kudos
2,550 Views
dharmeshkanzari
Contributor II

hello! thanks https://github.com/WaRP7/WaRP7-User-Guide/blob/80cc2de13a2dc21466a6ad9eedf4c5a143763dad/06-Chapter/Y...

when i write command 

ums 0 mmc 0

on i.mx7 terminal. it said command not found. 

can you help me??

0 Kudos
2,549 Views
fabio_estevam
NXP Employee
NXP Employee

Make sure you use an updated U-Boot version. You can use the latest 2016.11, for example, as it will contain the "ums" command.

Then you can load it via USB when the board is in Serial Download mode.

0 Kudos
2,548 Views
daiane_angolini
NXP Employee
NXP Employee

Please double check if you really don't have ums command on your u-boot. It's not an expected behavior.

Anyway, you can update u-boot by:

WaRP7-User-Guide/U-boot.adoc at master · WaRP7/WaRP7-User-Guide · GitHub 

and make sure you are aware of

WaRP7 possible brick and solution - i.MXDev Blog 

0 Kudos
2,548 Views
dharmeshkanzari
Contributor II

hello! actually i don't know how to open uboot terminal. i opened it and write

=> ums 0 mmc 0

then in ubuntu i operated operations 

fsl-image-machine-test-imx7s-warp-20161124-6.rootfs.sdcard.gz
dharmesh@dharmesh-HP-Notebook:~/a$ gunzip fsl-image-machine-test-imx7s-warp-20161124-6.rootfs.sdcard.gz
dharmesh@dharmesh-HP-Notebook:~/a$ sudo dd if=fsl-image-machine-test-imx7s-warp-20161124-6.rootfs.sdcard of=/dev/sdX
[sudo] password for dharmesh:
1384448+0 records in
1384448+0 records out
708837376 bytes (709 MB) copied, 1.60809 s, 441 MB/s
dharmesh@dharmesh-HP-Notebook:~/a$ 

after reboot. it has not yocto image

0 Kudos
2,548 Views
daiane_angolini
NXP Employee
NXP Employee

Here:

dharmesh@dharmesh-HP-Notebook:~/a$ sudo dd if=fsl-image-machine-test-imx7s-warp-20161124-6.rootfs.sdcard of=/dev/sdX

Are you replacing the *X* from dev/sdX to the right device number/letter?

0 Kudos
2,548 Views
dharmeshkanzari
Contributor II

how to find true *X* ?? 

0 Kudos
2,548 Views
daiane_angolini
NXP Employee
NXP Employee

Use dmesg.

type "dmesg" see the last lines. Then plug the sdcard, dmesg again and see the last line has changed. The last log shows the /dev/sdX kernel create to your sdcard.

0 Kudos
2,551 Views
dharmeshkanzari
Contributor II

after running that command. i didn't get login

0 Kudos