uuu LF_v6.1.36-2.1.0_images_IMX93EVK.zip fial

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uuu LF_v6.1.36-2.1.0_images_IMX93EVK.zip fial

Jump to solution
559 Views
Chihyu_Lin
Contributor III

Hi,

I would like to test latest image file from NXP, but got uuu [LIBUSB_ERROR_IO] error.

uuu.pnglsusb.png

0 Kudos
1 Solution
506 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Chihyu_Lin,

I hope you are doing well.

Can you please mention SOC silicon rev. ?

L6.1.36_2.1.0  only supports i.MX 93 EVK board (11x11 A1 silicon).
 
For i.MX 93 EVK board (11x11 A0 silicon), please use L6.1.22_2.0.0.
 
 
Thanks & Regards,
Dhruvit Vasavada

View solution in original post

3 Replies
541 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Chihyu_Lin,

I hope you are doing well.

Please make sure that you have set boot mode to serial download mode using the DIP switch.

Please refer to Table 4 — Boot Device Settings in i.MX 93 EVK Quick Start Guide  and Burn NXP Linux BSP Image Using Universal Update Utility (UUU)

Thanks & Regards,
Dhruvit Vasavada

0 Kudos
528 Views
Chihyu_Lin
Contributor III

Hi Dhruvit,

Thanks for your replied, but I did the same way to program LF_v6.1.22-2.0.0_images_IMX93EVK.zip without any problem. Only program v6.1.36 have this problem.

 

regards,

Chihyu Lin

0 Kudos
507 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Chihyu_Lin,

I hope you are doing well.

Can you please mention SOC silicon rev. ?

L6.1.36_2.1.0  only supports i.MX 93 EVK board (11x11 A1 silicon).
 
For i.MX 93 EVK board (11x11 A0 silicon), please use L6.1.22_2.0.0.
 
 
Thanks & Regards,
Dhruvit Vasavada