unit_tests/mxc_spi_test1.out on iMX53 QSB

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

unit_tests/mxc_spi_test1.out on iMX53 QSB

1,049件の閲覧回数
NeilSimpson
Contributor I
Has anyone tried using /unit_tests/mxc_spi_test.out to test out the SPI port(s) on the MX53 quicki start board?  Although the CSPI seems to be configured I get an error "cannot open the device" for all SPI device numbers I try.
タグ(1)
0 件の賞賛
3 返答(返信)

518件の閲覧回数
simone_cilli
Contributor I

Hello,

I'm stuck on the same problem.

/unit_tests/mxc_spi_test1.out -D 1 -b 16 1
Execute data transfer test: 1 1 1
Error:cannot open device (Maybe not present in your board?)

I don't see spi device in /dev/ although I added the driver during the kernel compilation.
How can I add the device?
Any news?

0 件の賞賛

518件の閲覧回数
chandiniindavar
Contributor IV

Hi Simone,

Even i am facing same problem.

Could you please tell me , Is you issue got solved ?

BR,

Chandini

0 件の賞賛

518件の閲覧回数
DougGibbs
Contributor I

Is there a SPI1.0 or spi_dev1.0 in the /dev directory.

I am in the process of building a kernel that gets spi to appear in /dev. Let me know if you have already figured out how to get that working.

0 件の賞賛