uStreamer porting for iMX8MM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uStreamer porting for iMX8MM

1,154 Views
r_trivedi123
Contributor IV

Hi,

I would like to use ustreamer with imx8 hardware encoder/decoder functionality. 

it is possible to use for imx8 ? can you provide any suggetion on this? 

https://github.com/pikvm/ustreamer, source that is used for raspberry pi board for streaming purpose.

Any help will be appreciable

Thanks & Regards

Labels (1)
0 Kudos
4 Replies

1,089 Views
r_trivedi123
Contributor IV

Hi @Bio_TICFSL ,

Any pointer on the above would be helpful.

--
Thanks

0 Kudos

1,080 Views
r_trivedi123
Contributor IV

Hi @Bio_TICFSL ,
Can you help ?

0 Kudos

1,130 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello r_trivedi123

 

If this ustreamer is µStreamer (ustreamer) is a lightweight and very quick server to stream MJPG video from any V4L2 device to the network, yes it can support by every i.MX8.

Regards

 

0 Kudos

1,124 Views
r_trivedi123
Contributor IV

Hi,

Thank you for your reply. 

Did test with µStreamer for iMX8MM board, and it works fine with  the camera input.

I have taken the dmesg logs for VPU logs entry  to check its usage and found that µStreamer is not using the VPU for encoding.

I found that  µStreamer uses the omx for encoding.

It is possible to get VPU(H/W) encoding with µStreamer? Any pointers in this ?

Any help will be appreciated. 

Regards

0 Kudos