Working to interface two OV5640 MIPI CSI cameras(MINISASTOCSI) to the imx8mqevk board. Per the schematic note, I've routed the I2C lines for the second camera to a separate I2C channel (I2C2). I made the adjustment to the device tree so both cameras are enabled.
If I have only one camera physically connected, both lines work. This confirms that device tree files work correctly with their respective cameras. However, when I have both cameras connected, the system freezes up on attempt to initialize second camera. Can the OV5640 drivers support two cameras?
Below is the message i get before it freezes:
[ 2.125015] i2c /dev entries driver
[ 2.132435] 0-003c supply DOVDD not found, using dummy regulator
[ 2.138514] 0-003c supply DVDD not found, using dummy regulator
[ 2.144480] 0-003c supply AVDD not found, using dummy regulator
[ 2.245928] random: fast init done
[ 3.266017] camera ov5640_mipi is found
[ 3.270015] 1-003c supply DOVDD not found, using dummy regulator
[ 3.276132] 1-003c supply DVDD not found, using dummy regulator
[ 3.282139] 1-003c supply AVDD not found, using dummy regulator
[ 4.418004] camera ov5640_mipi is found
[ 4.422874] mxc-mipi-csi2_yav 30a70000.mipi_csi1: mipi_csi2_probe
[ 4.429062] CSI: Registered sensor subdevice: mxc-mipi-csi2.0
[ 4.434867] mxc-mipi-csi2_yav 30a70000.mipi_csi: Remote device at /mipi_csi1@30a70000/port/endpoint1 XXX found
已解决! 转到解答。
Hi Bineyam,
My apologies, the fix is available in 4.9.123 i.MX8MM GA release. The relevant commit is linux-imx - i.MX Linux kernel
Make sure to properly configure reg and csi-id properties in ov5640_mipi DTS nodes. csi-id should be 0 for the first camera and 1 for the second one
Felix.
Hi Felix,
I am using 4.9.88 kernel. If I setup the second camera to use a separate i2c channel (and route the cables accordingly). After enabling both cameras in the device tree, the system boots up, finds the first camera, initializes it, finds the second camera, and hangs up on initializing the OS.
Bineyam
Hi Bineyam,
My apologies, the fix is available in 4.9.123 i.MX8MM GA release. The relevant commit is linux-imx - i.MX Linux kernel
Make sure to properly configure reg and csi-id properties in ov5640_mipi DTS nodes. csi-id should be 0 for the first camera and 1 for the second one
Felix.
Hello,
I apologize for the late answer. Let me investigate if the driver could support dual mipi-display camera. But how you are mentioning your case. Apparently is not supported.
Best Regards,
Diego.