Hi i am new to this,
I have two custom imx6DL boards.But only one difference between two boards(i.e board A is configured with SD1 and board B is configured with SD3).
So in uboot i changed for board B SD1 to SD3 and inmachine driver itself i changed to SD3.
Both boards are configured with same UART pins.(
MX6Q_PAD_SD3_DAT4__GPIO_7_1,
MX6Q_PAD_SD3_DAT5__UART2_TXD,)
My problem is Board A receive datas from microcontroller properly through UART.
But Board B is not at all receiving datas through UART from microcontroller.
I probe the receiver pin.But its toggle.
So whats the issue?how can i solve?
please help me to identify the issue..
With regards,
R.Giritharan
Why do you configure the SD3_DAT4 pin for GPIO function? To make it work as UART RX pin, you have to configure it as UART2_RXD.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------