top marking conventions of MCIMX535DVV1C and MCIMX258CJM4A ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

top marking conventions of MCIMX535DVV1C and MCIMX258CJM4A ?

1,676 Views
john_cheng
Contributor I

Dear All,

            i can't find the document which can supply the top marking conventions of MCIMX535DVV1C and MCIMX258CJM4A,

i have to provide for my customer, can anyone answer my question?

Best regards,

Labels (2)
Tags (3)
0 Kudos
4 Replies

1,192 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi John,

Please see IMX53 and IMX25 respective datasheets. For example, in the case of MCIMX535DVV1C, you can find the code in:

Document Number: IMX53CEC

Rev. 6, 03/2013

Section 1.1

Table 2.

We don't provide the complete convention meaning, but the characteristics of the device are explained there.

Best regards.

Jorge.

0 Kudos

1,192 Views
john_cheng
Contributor I

Dear Jorge,

             my customer want me to provide the complete the top marking on the chip. for example below image,but the datasheet don't explain completely.

top_mark.jpg

so, the top marking

2011722105937.jpg

you can look, there are so many charactrics, is there one datasheet which can provide completely conventions?

0 Kudos

1,192 Views
igorpadykov
NXP Employee
NXP Employee

Hi John

these markings conventions are closed from

public to avoid counterfeiting. You can obtain this info

from local marketing office. Also you can provide

marking details to check if parts are Freescale genuine

parts.

Best regards

igor

0 Kudos

1,192 Views
john_cheng
Contributor I

Dear igor,

       thanks, i try to contact with the local marketing office.

Best Regards,

John

0 Kudos