surfaceflinger can't start up

取消
显示结果 
搜索替代 
您的意思是: 

surfaceflinger can't start up

2,009 次查看
conteczxy
Contributor III

my environment : imx6q, android 8.0, kernel 4.9

on the console, there are lot of such messages,

init: starting service 'surfaceflinger'...
init: property_set("ro.boottime.surfaceflinger", "48482314005") failed: property already set
init: Failed to bind socket 'pdx/system/vr/display/client': No such file or directory
init: Failed to bind socket 'pdx/system/vr/display/manager': No such file or directory
init: Failed to bind socket 'pdx/system/vr/display/vsync': No such file or directory

who knows what is the problem?

Thanks,

标签 (2)
0 项奖励
1 回复

1,349 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Xiyuan

one can try solution suggested on

i.MX6 Android N7.1.2_2.0.0 boot up SurfaceFlinger crash 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励