nxp-wlan-sdk Fails Building in L5.4.47-2.2.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

nxp-wlan-sdk Fails Building in L5.4.47-2.2.0

4,938 次查看
marcelziswiler
Senior Contributor I

Attempting a Yocto Project build leads to the following build error:

⬢[user@toolbox build-xwayland-imx8mpevk]$ bitbake fsl-image-validation-imx
...
ERROR: nxp-wlan-sdk-git-r0 do_compile: oe_runmake failed
ERROR: nxp-wlan-sdk-git-r0 do_compile: Execution of '/home/user/imx-yocto-bsp_5.4.47-2.2.0/build-xwayland-imx8mpevk/tmp/work/aarch64-poky-linux/nxp-wlan-sdk/git-r0/temp/run.do_compile.3941835' failed with exit code 1:
/bin/sh: bc: command not found
make -C /lib/modules/5.9.11-100.fc32.x86_64/build M=/home/user/imx-yocto-bsp_5.4.47-2.2.0/build-xwayland-imx8mpevk/tmp/work/aarch64-poky-linux/nxp-wlan-sdk/git-r0/git/mxm_wifiex/wlan_src modules
make[1]: *** /lib/modules/5.9.11-100.fc32.x86_64/build: No such file or directory.  Stop.
make: *** [Makefile:412: default] Error 2
WARNING: /home/user/imx-yocto-bsp_5.4.47-2.2.0/build-xwayland-imx8mpevk/tmp/work/aarch64-poky-linux/nxp-wlan-sdk/git-r0/temp/run.do_compile.3941835:1 exit 1 from 'exit 1'

ERROR: Logfile of failure stored in: /home/user/imx-yocto-bsp_5.4.47-2.2.0/build-xwayland-imx8mpevk/tmp/work/aarch64-poky-linux/nxp-wlan-sdk/git-r0/temp/log.do_compile.3941835
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 56 build
| /bin/sh: bc: command not found
| make -C /lib/modules/5.9.11-100.fc32.x86_64/build M=/home/user/imx-yocto-bsp_5.4.47-2.2.0/build-xwayland-imx8mpevk/tmp/work/aarch64-poky-linux/nxp-wlan-sdk/git-r0/git/mxm_wifiex/wlan_src modules
| make[1]: *** /lib/modules/5.9.11-100.fc32.x86_64/build: No such file or directory.  Stop.
| make: *** [Makefile:412: default] Error 2
| ERROR: oe_runmake failed
| WARNING: /home/user/imx-yocto-bsp_5.4.47-2.2.0/build-xwayland-imx8mpevk/tmp/work/aarch64-poky-linux/nxp-wlan-sdk/git-r0/temp/run.do_compile.3941835:1 exit 1 from 'exit 1'
| ERROR: Execution of '/home/user/imx-yocto-bsp_5.4.47-2.2.0/build-xwayland-imx8mpevk/tmp/work/aarch64-poky-linux/nxp-wlan-sdk/git-r0/temp/run.do_compile.3941835' failed with exit code 1:
| /bin/sh: bc: command not found
| make -C /lib/modules/5.9.11-100.fc32.x86_64/build M=/home/user/imx-yocto-bsp_5.4.47-2.2.0/build-xwayland-imx8mpevk/tmp/work/aarch64-poky-linux/nxp-wlan-sdk/git-r0/git/mxm_wifiex/wlan_src modules
| make[1]: *** /lib/modules/5.9.11-100.fc32.x86_64/build: No such file or directory.  Stop.
| make: *** [Makefile:412: default] Error 2
| WARNING: /home/user/imx-yocto-bsp_5.4.47-2.2.0/build-xwayland-imx8mpevk/tmp/work/aarch64-poky-linux/nxp-wlan-sdk/git-r0/temp/run.do_compile.3941835:1 exit 1 from 'exit 1'
|
ERROR: Task (/home/user/imx-yocto-bsp_5.4.47-2.2.0/sources/meta-imx/meta-bsp/recipes-connectivity/nxp-wlan-sdk/nxp-wlan-sdk_git.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 4029 tasks of which 0 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
  /home/user/imx-yocto-bsp_5.4.47-2.2.0/sources/meta-imx/meta-bsp/recipes-connectivity/nxp-wlan-sdk/nxp-wlan-sdk_git.bb:do_compile
Summary: There were 10 WARNING messages shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

 

0 项奖励
回复
9 回复数

4,573 次查看
botondkardos
Contributor II

OK, fixed it. Use this how-to for modifying nxp-wlan-sdk_git.bb: https://www.yoctoproject.org/docs/1.6.1/kernel-dev/kernel-dev.html#incorporating-out-of-tree-modules

4,514 次查看
botondkardos
Contributor II
 

3,758 次查看
Jems-advantech
Contributor I

This patch works for me.

0 项奖励
回复

4,581 次查看
botondkardos
Contributor II

This is the real error:

make[1]: *** /lib/modules/5.9.11-100.fc32.x86_64/build: No such file or directory. Stop.

The Makefile tries to use the host machine's Linux sources while it ought to build against the target Linux. I'm in the middle of finding out what needs to be added to the recipe to use the target kernel.

0 项奖励
回复

4,673 次查看
yalefee
Contributor I

I have the same problem.not solved. Any NXP employee answer this?

0 项奖励
回复

4,659 次查看
marcelziswiler
Senior Contributor I

I never got any further comments from NXP. However, as stated earlier:

> The correct way to achieve this would be to properly add bc-native to the DEPENDS of any and all recipes requiring any such.

OK?

0 项奖励
回复

4,890 次查看
marcelziswiler
Senior Contributor I

Anybody from NXP dear to comment?

0 项奖励
回复

4,928 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi marcelziswiler,

You need install all needed packages as yocto build user guide.

/bin/sh: bc: command not found

 It shows that you did not install bc package.

 

Best Regards

Zhiming

0 项奖励
回复

4,921 次查看
marcelziswiler
Senior Contributor I

No, bc is not and never was a build host requirement. Please refer to section 21.2. Required Packages for the Build Host of the Yocto Project Reference Manual aka Mega-Manual:

https://www.yoctoproject.org/docs/current/mega-manual/mega-manual.html#required-packages-for-the-bui...

The correct way to achieve this would be to properly add bc-native to the DEPENDS of any and all recipes requiring any such. Thanks!

0 项奖励
回复