mx6q can support dual usb uvc camera in android 4.3 system?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

mx6q can support dual usb uvc camera in android 4.3 system?

跳至解决方案
1,529 次查看
mrleo
Contributor IV

Hi all,

    My custom board is mx6q board,I want support two usb uvc camera.

    One is ok for me,please help me how to support two usb uvc camera?

    Can it open at the same time?

Thanks,

Leo

0 项奖励
回复
1 解答
1,071 次查看
mrleo
Contributor IV

Hi Victor Linnik,

So two usb camera can't support in android.But can support in linux system.

Thanks Very much!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,072 次查看
mrleo
Contributor IV

Hi Victor Linnik,

So two usb camera can't support in android.But can support in linux system.

Thanks Very much!

0 项奖励
回复
1,071 次查看
b36401
NXP Employee
NXP Employee

You can connect 2 USB cameras to i.MX6 fine.

Please refer "Using a USB Camera with GStreamer" document

https://community.freescale.com/docs/DOC-93688

regarding connecting the cameras.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复