mounting usbfs on /proc/bus/usb failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mounting usbfs on /proc/bus/usb failed

ソリューションへジャンプ
4,651件の閲覧回数
小川崇
Contributor II

Greetings,

I have a problem when I boot my i.MX53 ARD board from SD card.

The error occurs when udev  is trying to mount usbfs as shown below.

                .

                .

Mounting /proc and /sys

Starting the hotplug events dispatcher udevd

Synthesizing initial hotplug events

Setting the hostname to freescale

Mounting filesystems

mount: mounting usbfs on /proc/bus/usb failed: No such file or directory

Starting inetd:

starting pid 2117, tty '': '/sbin/getty -L ttymxc0 115200 vt100'

                  .

                  .

I want to fix this error.
but I don't know how to fix this problem.
I appreciate if someone can help me to solve it

Regards,

takashi.

Original Attachment has been moved to: boot.log.zip

ラベル(1)
0 件の賞賛
返信
1 解決策
2,667件の閲覧回数
txbest
Contributor II

Are you sure that is a problem?The log that you given above saids usbfs not mount Ok!

Did you connect your board to PC via USB_otg?and of cource you have to config your PC and your board ,they must be in the same IP area!

If you can login your linux system , that is to say ,it is not a problem.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,668件の閲覧回数
txbest
Contributor II

Are you sure that is a problem?The log that you given above saids usbfs not mount Ok!

Did you connect your board to PC via USB_otg?and of cource you have to config your PC and your board ,they must be in the same IP area!

If you can login your linux system , that is to say ,it is not a problem.

0 件の賞賛
返信