Hello...
I've been able to hack my way through this build so far with a little help from Google and this forum- but this one has me stumped... somehow the Makefile is interpreting "no" as a command and there is no "no" that I've ever heard of.
I see that it is building "demos"- probably not needed- would anyone have a suggestion about possibly removing the demos section from the Makefile??
Output below:
Making all in demos
make[2]: Entering directory `/home/robb/ARM_board/L2.6.35_11.09.01_ER_source/ltib/rpm/BUILD/gtk+-2.14.3/demos'
no --raw --build-list \
apple_red ./apple-red.png \
gnome_foot ./gnome-foot.png \
> test-inline-pixbufs.h \
|| (rm -f test-inline-pixbufs.h && false)
/bin/bash: no: command not found
make[2]: *** [test-inline-pixbufs.h] Error 1
make[2]: Leaving directory `/home/robb/ARM_board/L2.6.35_11.09.01_ER_source/ltib/rpm/BUILD/gtk+-2.14.3/demos'
make[1]: *** [all-recursive] Error 1
make[1]: Leaving directory `/home/robb/ARM_board/L2.6.35_11.09.01_ER_source/ltib/rpm/BUILD/gtk+-2.14.3'
make: *** [all] Error 2
error: Bad exit status from /home/robb/ARM_board/L2.6.35_11.09.01_ER_source/ltib/tmp/rpm-tmp.26722 (%build)
RPM build errors:
Bad exit status from /home/robb/ARM_board/L2.6.35_11.09.01_ER_source/ltib/tmp/rpm-tmp.26722 (%build)
Build time for gtk2: 78 seconds
Failed building gtk2
f_buildrpms() returned an error, exiting
traceback:
main:560
Started: Thu May 3 14:22:40 2012
Ended: Thu May 3 14:23:58 2012
Elapsed: 78 seconds
These packages failed to build:
gtk2