is there any sample, iMX8M as a USB device?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

is there any sample, iMX8M as a USB device?

755 Views
mm2021
Contributor III

a simple sample, under linux, with source code.

Thanks!

0 Kudos
3 Replies

751 Views
mm2021
Contributor III

seems that iMX8M mini board is just used as USB host? Can it be used as a USB device?

0 Kudos

748 Views
b36401
NXP Employee
NXP Employee

i.MX8MMini processor has 2 USB OTG controller cores.

0 Kudos

746 Views
mm2021
Contributor III

Thanka for your reply.

Is there any example or application note as USB device, like UAC, etc.

0 Kudos