Hi
We got PIMX9352CVVXMAB chip, using uuu download 6.1.22 uboot got LIBUSB_ERROR_PIPE. Windows could got chip, any idea of this kind of error?
After running DDR TRIM and re-compile Uboot the Device could be program and bootup.
Hello, I hope you are doing well.
Could you please share me more about your hardware setup? Such as board used (custom/EVK), modifications, etc.
Best regards.
Hi,
This is custom board, but use same i2c, PMIC, DDR, uart1 and USB1 as EVK, some GPIO setting is different,and eMMC size is 4GB. We checked those power voltage.
Got it, could you please try with the next command?
uuu -b emmc_all imx-boot-<censored part>-sd.bin-flash_singleboot
never-displayed