imx8ulp lpddr3 tool not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8ulp lpddr3 tool not working

244件の閲覧回数
louisliu
Contributor I

We are bring a new custom IMX8ULP board with LPDDR3.  The DDR tools (https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software:IMX-SW --> Other Resources --> Tools --> DDR Tools" can recognized the board (USB-HID OK).  However, when we try to load the scripted generated by the "MX8ULP_LPDDR3_RPA.xls" spreadsheet, the APP give a "[ERROR] DDR type is incorrect!" message.  Can you help us with this issue? Thanks

 

Louis Liu

 

#imx8ulp  #lpddr3

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

214件の閲覧回数
johnsonwu
NXP Employee
NXP Employee

Hi @louisliu,

Please use this .ds file and you can try this file in stress test tool which you get from the support team,

If you use the lpuart6 to do stress test, you could get the log as the attachment.

Best Regards,

Johnson  

0 件の賞賛
返信

159件の閲覧回数
louisliu
Contributor I

Hi Jonhson,

 

Sorry the the late response, there were a lot of things going on last week.

First, the script you included does not work the the current "mx8ulp_ddr_tool" that is currently on the web page.  (We can not find version information anywhere in the application)

We are now picking up support from FAE.  We got a new version "mx8ulp_ddr_tool" which successfully create the timing file.  However, after adding parameters to u-boot, the uuu tools only past stage 1 of the process, where the chip failed to initialized/boot.  We can not isolate the problem at this moment.  We are debugging the hardware with the AE support right now.

I think this issue can be closed for now.

Thanks for all the support.

0 件の賞賛
返信