imx8mq composed video on dual display

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mq composed video on dual display

1,208 Views
subhasishghosh
Contributor II

Hi,

We are trying to display two overlayed composed videos in dual display configuration on the i.MX8MQ EVM.

One of the display is directly HDMI and the other is over MIPI -DSI to HDMI ADV7535 converter.

The gstreamer commands are as follows:

gst-launch-1.0 glvideomixer name=m \
sink_1::xpos=0 sink_1::ypos=0 sink_1::width=1920 sink_1::height=1080 ! \
videorate ! video/x-raw,framerate=30/1 ! \
kmssink can-scale=false sync=true \
filesrc location=bbb_sunflower_1080p_30fps_normal_x264_1m.mp4 ! qtdemux ! h264parse ! vpudec use-vpu-memory=true ! queue ! m.sink_1

gst-launch-1.0 glvideomixer name=m \
sink_3::xpos=0 sink_3::ypos=0 sink_3::width=1920 sink_3::height=1080 ! \
videorate ! video/x-raw,framerate=30/1 ! \
glimagesink sync=false enable-last-sample=false render-rectangle='<0,0,1920,1080>' \
filesrc location=bbb_sunflower_1080p_30fps_normal_x264_1m.mp4 ! qtdemux ! h264parse ! vpudec use-vpu-memory=true ! queue ! m.sink_3

While running these commands together, we observe that the frame rates reduce and the kmssink video starts to stutter or tear.

If we execute gputop -m ddr, the read-cycles ~ 3500 and writw-cycles ~ 2200 (MB).

Can we play two independent composed video on the kms and wayland sink.

Is the DDR or GPU bandwidth maxing out. How can we measure the current GPU load and what is the expected maximum DDR r/w cycles.

We are using the i.MX8MQ EVM and Linux 4.19.35 BSP.

Labels (1)
1 Reply

1,060 Views
igorpadykov
NXP Employee
NXP Employee

Hi subhasish

for  playing video on different displays one can check

i.mx8M EVK board encoder and decoder 

Use linux tool "perf" to get the ddr bandwidth data

perf stat -I 1000 -a -e ddr0/read-cycles/,ddr0/write-cycles/

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply