imx8mmini uuu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8mmini uuu

957 Views
jieh朱
Contributor III

I downloaded uuu.pdf. I built yocto to compile fsl-image-qt5-validation-imx-imx8mmevk.sdcard.bz2 and imx-boot-imx8mmevk-sd.bin-flash_evk through uuu.exe he can burn to imx8mminiemmc. Imx8mmini can also be started, but I git clone uboot and kernel source. The compiled binaries are u-boot-nodtb.bin and fsl-imx8mm-evk.dtb and rooffs.tar.bz2 is not .sdcard.bz2 and .bin-flash_evk
what should I do

0 Kudos
1 Reply

757 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

For this case, the easiest way would be to manually flash them to the SD card using a Linux PC, please see i.MX_Linux_User's_Guide.pdf section 4.3 Preparing an SD/MMC card to boot, this because Yocto creates the .sdcard file by default it is not created when built in standalone.

 

Hope this helps,

Best regards,

Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos