imx8dx libsdl2 color display problem

取消
显示结果 
搜索替代 
您的意思是: 

imx8dx libsdl2 color display problem

217 次查看
songhongliang
Contributor II

HI

I am trying to use libsdl2, but the windows created with SDL2 on the imx8dx development board are showing wrong colors. Compared with using the same program on ubuntu, the display on Ubuntu is normal, and the color displayed on the imx8dx development board is always wrong. I added in conf/local.conf IMAGE_INSTALL_append += "libsdl2 libsdl2-net libsdl2-mixer libsdl2-ttf libsdl2-image"

 

Thanks!

0 项奖励
2 回复数

186 次查看
Sanket_Parekh
NXP Employee
NXP Employee

Hi @songhongliang 

I hope you are doing well.

Please try with libsdl.

Thanks & Regards

Sanket Parekh

0 项奖励

215 次查看
songhongliang
Contributor II

hi

Attached is the comparison shown above on Ubuntu and imx8dx

Thanks

标记 (1)
0 项奖励