imx8 make an SD card to start the system.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8 make an SD card to start the system.

2,245件の閲覧回数
191782021
Contributor I

I need to make an SD card to start the system. I used the following 4.3 method to cause the following problems after the startup of uboot. Please help me thank you

pastedImage_2.png

uboot log

U-Boot 2018.03 (Jun 04 2020 - 18:14:12 +0800)

CPU: Freescale i.MX8MQ rev2.1 1500 MHz (running at 1000 MHz)
CPU: Commercial temperature grade (0C to 95C) at 41C
Reset cause: POR
Model: Freescale i.MX8MQ 
DRAM: 2 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

Failed (-5)
No panel detected: default to HDMI
Display: HDMI (1280x720)
In: serial
Out: serial
Err: serial

BuildInfo:
- ATF 1cb68fa
- U-Boot 2018.03

SF: Detected w25q64dw with page size 256 Bytes, erase size 64 KiB, total 8 MiB
eth0 MAC address is invailed !!
Use default MAC adderss:0x00:0x04:0x9F:0x01:0x30:0xE0
flash target is MMC:1
Net: eth0: ethernet@30be0000
cannot get the partion info for misc
idx 0, ptn 0 name='gpt' start=0 len=2048
idx 1, ptn 0 name='' start=0 len=0
idx 2, ptn 0 name='m4_os' start=10240 len=512
idx 3, ptn 0 name='all' start=0 len=7774208
idx 4, ptn 0 name='bootloader0' start=66 len=8192
idx 5, ptn 1 name='mmcsdb1' start=16384 len=131072
idx 6, ptn 2 name='mmcsdb2' start=147456 len=7626752
Cannot find partition 4080
do_raw_read failed, ret 1
read_bootctl, bcb_rw_block read failed
read command failed
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
cannot get the partion info for fbmisc
idx 0, ptn 0 name='gpt' start=0 len=2048
idx 1, ptn 0 name='' start=0 len=0
idx 2, ptn 0 name='m4_os' start=10240 len=512
idx 3, ptn 0 name='all' start=0 len=7774208
idx 4, ptn 0 name='bootloader0' start=66 len=8192
idx 5, ptn 1 name='mmcsdb1' start=16384 len=131072
idx 6, ptn 2 name='mmcsdb2' start=147456 len=7626752
fastboot_get_lock_stat: error in get mmc part
fsl_read_from_partition_multi: no misc partition
idx 0, ptn 0 name='gpt' start=0 len=2048
idx 1, ptn 0 name='' start=0 len=0
idx 2, ptn 0 name='m4_os' start=10240 len=512
idx 3, ptn 0 name='all' start=0 len=7774208
idx 4, ptn 0 name='bootloader0' start=66 len=8192
idx 5, ptn 1 name='mmcsdb1' start=16384 len=131072
idx 6, ptn 2 name='mmcsdb2' start=147456 len=7626752
avb_ab_flow.c:105: ERROR: Error reading A/B metadata.
fsl_avb_ab_flow.c:603: ERROR: I/O error while loading A/B metadata.
fsl_write_to_partition: no misc partition
idx 0, ptn 0 name='gpt' start=0 len=2048
idx 1, ptn 0 name='' start=0 len=0
idx 2, ptn 0 name='m4_os' start=10240 len=512
idx 3, ptn 0 name='all' start=0 len=7774208
idx 4, ptn 0 name='bootloader0' start=66 len=8192
idx 5, ptn 1 name='mmcsdb1' start=16384 len=131072
idx 6, ptn 2 name='mmcsdb2' start=147456 len=7626752
avb_ab_flow.c:134: ERROR: Error writing A/B metadata.

3 返答(返信)

2,119件の閲覧回数
191782021
Contributor I

flash.bin Due to production error, it can be made once again

0 件の賞賛

2,119件の閲覧回数
karangajjar
Senior Contributor II

Hi JCon St,

Can you let us know which version of iMX Linux User Guide are you following?

After partitioning the card, please verify that you have copied Bootloader, Kernel image & dtb, and root filesystem to the card. Also, make sure the boot switches on the EVK board are set to boot from SD card. 

Download the iMX Linux User Guide and iMX Yocto User Guide from this link.

Regards,

Karan Gajjar

2,119件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Good!