imx8 DDR stress tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8 DDR stress tool

1,802 次查看
kayiyeh
Contributor II

I tried to run ddr stress tool on my imx8mqevk borad. I follow the user guild, connect two USB cables, start the tool with administration mode. Then search UART, connect it, load the script, download it. The I got the screen as attached. The calibration or stress buttons turned pale, and the functions are not available. Could anyone tell me what's going wrong? 

标记 (2)
0 项奖励
回复
2 回复数

1,507 次查看
karangajjar
Senior Contributor II

Hi Ka-Yi Yeh

We tried ddr stress tool on imx8mqevk borad,The steps you are following are correct but in LOAD DDR SCRIPT section you have to mention .ds file which is given in script/mx8m/.ds.

Let us know in case of any concerns.

 

Regards,

Karan Gajjar

0 项奖励
回复

1,507 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ka-Yi Yeh

from log seems ver.1.0 tool used, please try with latest ver.3.0 tool

https://community.nxp.com/docs/DOC-340179 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复