imx7d how to use USB OTG as a slave device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx7d how to use USB OTG as a slave device

496件の閲覧回数
864535720
Contributor II

imx7d how to use USB OTG as a slave device
Hello everyone, I am using the MCIMX7SABRE development board provided by the NXP official website. Due to the functional requirements of the product, we need to use USB_OTG1 as a slave device and USB_OTG2 as a master device. Now USB_OTG2 can be used as a master device, but USB_OTG1 cannot always be used as a slave device. At the same time, I found that when I use mfgtools for programming, USB_OTG1 is used as a slave device. How do I configure it to make USB_OTG1 a slave device?

ラベル(1)
0 件の賞賛
1 返信

410件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

 See below, please!

pastedImage_2.png

1. USB OTG ID should be pulled up HIGH

2. USB OTG VBUS should be supplied by external PC USB via USB cable.

then usb otg will work at device mode.

Have a nice day!

BR,

Weidong

0 件の賞賛