imx6 u-boot ltib nothing on minicom

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 u-boot ltib nothing on minicom

Jump to solution
1,017 Views
alexandredel
Contributor I

Hello everybody

I am trying to flash a u-boot on my sabrelite board, however, when i use imx loader with the u boot created by ltib, nothing appear on minicom. When i try with the u-boot.bin, it succeed but there is nothing on the minicom's prompt, and when i try with the u-boot, it says:

unknown load address

HAB security state: development mode (0x56787856)

And of course, there is nothing on the prompt.

Do you have an idea how to fix this?

Thanks

Alexandre

Labels (1)
0 Kudos
1 Solution
622 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alexandre

actually sabrelite board uses own bootloaders and special methods for flashing them.

Please refer to excellent help resource below and post issue if this will not help

on boundary devices forum

http://eewiki.net/display/linuxonarm/i.MX6x+SABRE+Lite+SPI+Flash+Recovery

http://boundarydevices.com/community/

Best regards

chip
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
623 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alexandre

actually sabrelite board uses own bootloaders and special methods for flashing them.

Please refer to excellent help resource below and post issue if this will not help

on boundary devices forum

http://eewiki.net/display/linuxonarm/i.MX6x+SABRE+Lite+SPI+Flash+Recovery

http://boundarydevices.com/community/

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos