imx6 sabre SD HDMI video output with some distortion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 sabre SD HDMI video output with some distortion

462 Views
julianooliveira
Contributor I

I'm developing a product with imx6 sabre sd board with android Jelly bean 4.3. The main issue that I need to solve is about using the HDMI. I'm successfully develop an app to show different contents in the local lcd and in the hdmi, but if I try to show  a video throug the hdmi the output show some distortions (see picture). I investigate the parameter bits_per_pixel, and the value used is 16, i tried use other values to this parameter but without success, any suggestion of how to fix it? The same video running on local lcd don't show the same problems.

distorcao.jpg

Labels (1)
Tags (2)
0 Kudos
1 Reply

369 Views
igorpadykov
NXP Employee
NXP Employee

Hi Juliano

one can try Demo Images from link

i.MX 6 Series Software and Development Tool|NXP 

also try to change hdmi monitor and use quality hdmi cable

with good shielding.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos