[imx6] RS485 could be supported on Imx6 series ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[imx6] RS485 could be supported on Imx6 series ?

ソリューションへジャンプ
8,077件の閲覧回数
keres_kim
Contributor II

Hi imx-developers,

Good day !

It's simple. Could imx6 chipset support RS485 ?

There are many related questions posted on this community about RS485.

Many patch codes exist as well but I not sure which one would be trusted.

Would you somebody tell us which patch code works well on rs485 ?

thank you. 

0 件の賞賛
返信
1 解決策
4,956件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi keres

RS485 is currently not supported by the imx serial driver, however

some folks seems added RS485 support to the imx serial driver.

http://marc.info/?l=linux-kernel&m=142366865609389&q=raw

http://www.spinics.net/lists/linux-serial/msg15795.html

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,957件の閲覧回数
raje_embd13
Contributor I

I had similar requirement right now. Can help on this.  Is any patch which support RS485 on Imx6 processor ?

0 件の賞賛
返信
4,957件の閲覧回数
marcocavallini
Contributor V
0 件の賞賛
返信
4,959件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi keres

RS485 is currently not supported by the imx serial driver, however

some folks seems added RS485 support to the imx serial driver.

http://marc.info/?l=linux-kernel&m=142366865609389&q=raw

http://www.spinics.net/lists/linux-serial/msg15795.html

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
4,957件の閲覧回数
keres_kim
Contributor II

Dear Igor,

Thank you for your response.

Patch code from "Marc" is working well.

http://marc.info/?l=linux-kernel&m=142366865609389&q=raw

RS485 TX data has verified successfully,But not RX. I'm still checking on it.

Have a nice day ~~

0 件の賞賛
返信
4,957件の閲覧回数
LPs
Contributor III

Hi Kim,

   did you managed to make the RX working?

0 件の賞賛
返信