imx53的IPU的两个通道就是指LVDS的两个通道么?要是我想两路LVDS和一路TTL上同时显示,但是IPU只有两个通道,这样可以实现么

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx53的IPU的两个通道就是指LVDS的两个通道么?要是我想两路LVDS和一路TTL上同时显示,但是IPU只有两个通道,这样可以实现么

Jump to solution
764 Views
wlwwlw
Contributor I

如标题

0 Kudos
1 Solution
558 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

iMX53 IPU has two DI (Display interface) which can support two different displays, but for LVDS, if the two LVDS displays are same, they can connected two LVDS port but get data from same IPU DI, in this case, another display can be supported on another DI. The limitation for this use case: the two LVDS panels are same timing, same resolution, and show same content.

View solution in original post

0 Kudos
2 Replies
558 Views
YixingKong
Senior Contributor IV

Wlw, if your questions had been answered please clicking Correct Answer/Helpful Answer. We will close the Di if not response in 3 days.

Thanks,

Yixing

0 Kudos
559 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

iMX53 IPU has two DI (Display interface) which can support two different displays, but for LVDS, if the two LVDS displays are same, they can connected two LVDS port but get data from same IPU DI, in this case, another display can be supported on another DI. The limitation for this use case: the two LVDS panels are same timing, same resolution, and show same content.

0 Kudos