iMXRT reboot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,486件の閲覧回数
mspenard603
Contributor IV

How does one reboot, in software, an iMXRT1062?

0 件の賞賛
返信
1 解決策
1,382件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Mike,

Thanks for your reply.
it can make the RT1062 reboot via calling NVIC_SystemReset();
I've attached a sample code that inherits from the hello_world demo in the SDK library. And the testing result is also presented below.

/*
 * Copyright (c) 2013 - 2015, Freescale Semiconductor, Inc.
 * Copyright 2016-2017 NXP
 * All rights reserved.
 *
 * SPDX-License-Identifier: BSD-3-Clause
 */

#include "fsl_device_registers.h"
#include "fsl_debug_console.h"
#include "board.h"

#include "pin_mux.h"
#include "clock_config.h"
/*******************************************************************************
 * Definitions
 ******************************************************************************/


/*******************************************************************************
 * Prototypes
 ******************************************************************************/

/*******************************************************************************
 * Code
 ******************************************************************************/
/*!
 * @brief Main function
 */
int main(void)
{
    char ch;

    /* Init board hardware. */
    BOARD_ConfigMPU();
    BOARD_InitPins();
    BOARD_BootClockRUN();
    BOARD_InitDebugConsole();

    PRINTF("\r\n hello world.\r\n");

    while (1)
    {
        ch = GETCHAR();
        if(ch == 'y')
        {
          NVIC_SystemReset();
        }
        PUTCHAR(ch);
    }
}

pastedImage_1.png

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
1,382件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Mike Spenard,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Actually, I'm not very clear about your question, please you can clarify it.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,382件の閲覧回数
mspenard603
Contributor IV

Sure, I'm simply looking for a way to make a call that reboots the MCU.

0 件の賞賛
返信
1,383件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Mike,

Thanks for your reply.
it can make the RT1062 reboot via calling NVIC_SystemReset();
I've attached a sample code that inherits from the hello_world demo in the SDK library. And the testing result is also presented below.

/*
 * Copyright (c) 2013 - 2015, Freescale Semiconductor, Inc.
 * Copyright 2016-2017 NXP
 * All rights reserved.
 *
 * SPDX-License-Identifier: BSD-3-Clause
 */

#include "fsl_device_registers.h"
#include "fsl_debug_console.h"
#include "board.h"

#include "pin_mux.h"
#include "clock_config.h"
/*******************************************************************************
 * Definitions
 ******************************************************************************/


/*******************************************************************************
 * Prototypes
 ******************************************************************************/

/*******************************************************************************
 * Code
 ******************************************************************************/
/*!
 * @brief Main function
 */
int main(void)
{
    char ch;

    /* Init board hardware. */
    BOARD_ConfigMPU();
    BOARD_InitPins();
    BOARD_BootClockRUN();
    BOARD_InitDebugConsole();

    PRINTF("\r\n hello world.\r\n");

    while (1)
    {
        ch = GETCHAR();
        if(ch == 'y')
        {
          NVIC_SystemReset();
        }
        PUTCHAR(ch);
    }
}

pastedImage_1.png

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------